Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! undefined reference to `CNFG0_Fifo_RX' & more

Hello Everyone, update: I Worked it out :), forgot to declare the function. must of deleted it and forgot about it.I'm having an issue with finishing a build, i've modified the low level drivers for Can and named the callback functions ( from the fil...

0693W000000UMqxQAG.png 0693W000000UMseQAG.png 0693W000000UMv9QAG.png 0693W000000UMvYQAW.png
AMeta by Associate II
  • 1449 Views
  • 1 replies
  • 1 kudos

Resolved! How to test SPC582B CAN Communication?

Hello, ​I have two board with SPC582B 64Pin.​i want to test CAN communication each other. ​i did import sample what "SPC582BxxRLA CAN Test Application for Discovery"​and i want to use CAN port - 1, 2​i don't know how can i make code.​/* SPC5 RLA...

0693W000000UxCpQAK.png 0693W000000UxCuQAK.png
BKIM.11 by Associate
  • 1800 Views
  • 1 replies
  • 0 kudos

Resolved! WAKEUP not working in SPC560B

I am using SPC560B microcontroller, I want to program in such a way that the module should produce a wakeup interrupt ever 0.1S once. What is the value to be loaded in RTCVAL field in the RTCC register for 0.1s interrupt.I have used a clock source of...

SEphr by Associate II
  • 1806 Views
  • 2 replies
  • 0 kudos

Resolved! How to check whether the SPC560B54L5 EVB IS IN STANDBY mode or not?

Hello,I am trying to make SPC560B54L5 EVB in low power mode that is STANDBY mode.The measured current in normal RUN0 mode is 143 mA whereas while keeping in STANDBY mode, it is around 92 mA. But as per the AN3316 Application note the max current cons...

0693W000000U6AvQAK.jpg
rpoon by Associate II
  • 1661 Views
  • 1 replies
  • 0 kudos

Resolved! How to use SPC560b54l5 discovery board to flash spc560b50l5 chip?

HI all, I am Ragu, and I need to flash SPC560b50l5 chip using SPC560b54l5 discovery board. I use PLS adapter setting in document as they mentioned but it not works?. Below I attached JTAG connection circuit diagram which I use. I probe the ...

Rpala.1 by Associate II
  • 2450 Views
  • 2 replies
  • 0 kudos

Resolved! How can I configure Simulink to compile for the SPC58-4B?

I have a SPC584B-DIS discovery board, and I can see that on the Matlab website it's listed as being supported hardware for Simulink.I have been trying to understand how exactly it should work though. I can see that most (all?)of the Simulink blocks a...

OGisl.1 by Associate
  • 2806 Views
  • 3 replies
  • 0 kudos

How to include Flash Driver into SPC5Studio project?

Hi,I am trying to include Flash Driver component into my project of SPC560B50L1.I have added it from available components and it appeared in project as shown on attached screenshot.Then I wrote simple procedure, but linker says that flash driver's fu...

0690X00000ButzFQAR.png
Yannek by Associate III
  • 5044 Views
  • 7 replies
  • 0 kudos

configure GPIOs at runtime; based on CAN message

HI, I am using SPC560b54l5 discovery board,I want to configure multiple GPIOs at runtime; based on the message received from CAN, when I configure particular pin as I/O by using pal_setgroupmode function but it not works, can anyone face this issue? ...

Rpala.1 by Associate II
  • 1404 Views
  • 1 replies
  • 0 kudos