| Subject | Author | Posted | |
|---|---|---|---|
|
Since in the RM0483 Reference manual SR5E1x 32-bit Arm® Cortex®-M7 architecture microcontroller for...
| 2026-06-08 9:49 AM | ||
|
StellarStudio 9.1 (LEDS-2) — Release Notes
StellarStudio 9.1.0 (LEDS-2) version is officially...
| 2026-06-08 6:03 AM | ||
|
The STEVAL-TTM004V1 board has no response when connected to a 5V power supply; J5 is connected ...
| 2026-05-26 9:50 AM | ||
|
Hi Team, We have a requirement to lock the JTAG for the SPC58NN controller. Could anyone please s...
| 2026-05-24 11:38 PM | ||
|
Hello, I am facing an issue with flashing firmware to MCU SPC560P50L3 using StellarLINK probe. I h...
| 2026-05-24 8:51 PM | ||
|
Hello! I am studying the SPC58NH92E7. I'd like to clarify some terms and definitions. Below, I’ll...
| 2026-05-20 11:33 PM | ||
|
Are HAL drivers and/or LL driver available for SR5E1E3 or E1E5? Where can be found? I saw some HA...
| 2026-05-20 6:11 AM | ||
|
Hi, I am creating project in STM32 StellarStudio for SR5E1. But the Makefile might be running ...
| 2026-05-19 6:48 AM | ||
|
Dear Team, We are planning to use the SPC560B50L1B4E0X MCU for project. We would like to get offi...
| 2026-05-13 3:28 AM | ||
|
My code is as follows. volatile uint8_t d_deadcode = 0U;
void sleepManagement(void)
{
if...
| 2026-05-06 2:42 AM | ||
|
I am developing using AutoDevKit and SPC582Bxx. When the device wakes up from STANDBY0 to WKPU, it...
| 2026-05-03 3:17 AM | ||
|
Hello,
I updated my StellarStudio from 9.0.0 to 9.0.2 and pin configuration editor stopped workin...
| 2026-04-28 4:21 AM | ||
|
Hi Do any example bootloader files exist for the SR5E1E5 micro series. I can see that there ar...
| 2026-04-28 3:30 AM | ||
|
SPC5 Flash Programmer SPC5 Flash Programmer 2.8.1 Fail to connect to SPC564 via UART!, wh...
| 2026-04-21 3:22 AM | ||
|
Hi Everyone, I have been using SPC563M64L7 MCU Discovery board and created simple application util...
| 2026-03-20 5:44 AM | ||
|
The SR5E1E7 program written with a trimmed library, Makefile, and blank project file has locked up ...
| 2026-03-17 12:51 AM | ||
|
Hi, I'm using SPC560D-Discovery and want to boot it via UART: I've closed J12 and J13 according to ...
| 2026-01-30 4:52 AM | ||
|
Hello Community, I would like to understand in general how to activate a peripheral interface suc...
| 2026-01-23 6:38 AM | ||
|
Dear community, I am currently working on the FlexRay driver and wondered, where do I have to put ...
| 2026-01-22 11:33 PM | ||
|
How can I boot my own application on sr5e1? I read about DCF and BAF but it is not really clear wh...
| 2026-01-15 6:58 AM |