2020-02-19 3:58 AM - last edited on 2025-03-20 3:54 AM by Andrew Neil
HI, I am using SPC560b54l5 discovery board,
I want to configure multiple GPIOs at runtime; based on the message received from CAN, when I configure particular pin as I/O by using pal_setgroupmode function but it not works, can anyone face this issue?
please help me.
with regards,
Ragu.
2020-02-28 9:40 PM
Hi all, At-least I found one way to do configure GPIOs mode(input or output) at run time. I found that static const spc_siu_init_t spc_siu_init[] structure present in board.c file contains all our pins configuration but it is a constant structure; so, I made one copy of the same file and change the constant structure to ordinary structure and the I change input as output and vice-versa by doing on register level writing on SIU register like this SIU.PCR[spc_siu_run[PIN_GPIO0].pcr_index].R = (iomode_t)(PAL_MODE_OUTPUT_PUSHPULL); This will configure GPIO0 as output, initially I configure as input.
Thq
with Regards,
Ragu
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.