Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! SPC5 interfacing with NAND

Hi All,is there any mcu in SPC5 family with interface for unmanaged raw NAND chips, e. g. External Bus Interface or something else? I've checked modern gen. datasheets and haven't found any mentions about NAND. Thanks for any help

pbori.1 by Associate
  • 1193 Views
  • 1 replies
  • 0 kudos

Resolved! SPC5Studio 5.8.1 instalation - not found make.exe

New installation from scratch of SPCStudio 5.8.1 gives error that make is not found. I start a project with GCC and cant build the project. I cant find the make.exe nowhere except the hightec plugin folders. When I add those folders i got other error...

PParf.1 by Associate
  • 4608 Views
  • 6 replies
  • 0 kudos

Resolved! I try to find a way use LINFlexD (no use filter - Slave Mode)

Hello.I have a using eval board : SPC58EC-DISP.​I try to receive all packet (slave mode) just like DAQ. SPC STUDIO support LinFlexD example only using filter.I think that lin_lld.c - spc5xx_lin_rxi_interrupt (SPC STUDIO Example) is need to modified.P...

MSeo.9 by Associate
  • 1226 Views
  • 1 replies
  • 0 kudos

Resolved! DMA re configuration

Hi All,We are using different ADC group to access DMA channel. We have 3 ADC groups, Group1 ADC channel need to read continuously. So it should stop the other ADC channels to accessing the DMA. If it is accessing, it should stop it and reconfigure wi...

Resolved! How to generate UART RX INTERRUPT WITH SPC560PXX

Hello All,I am working on UART on SPC560p Discovery board. I can transmit the data but unable to receive the data. I want to receive byte by interrupt method to avoid blocking.Please guide me with Rx interrupt initialization so that I can use"stat...

Pradnya by Associate II
  • 1191 Views
  • 1 replies
  • 0 kudos

Resolved! Setting up program from scratch ?

Hey AllFairy new to SPC5 development, coming from st's 32bit standard Micro controllers.I have a few questions on the process to creating a project from scratch1) Are we meant to just load the example projects and modify them according to our needs a...

0693W000000UA3tQAG.jpg 0693W000000UA3ZQAW.jpg
AndreasPA by Associate III
  • 1654 Views
  • 2 replies
  • 1 kudos

Resolved! UDE folder is not creating after project build

Hi All,I'm using SPC560P development board in my project. Using SPC5 studio for code development and UDE for debugging purpose. I built the project, but it is not creating UDE folder in the project .How I can create or update my UDE folder after eve...