STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Installation Issues - Infinite Loop

I've got a brand new VM running Windows 11 pretty much off the shelf. I can install and run Cube IDE but when I try to install the STM32CubeProgrammer (64 bit version) I get into an infinite loop where the following happens:- It opens the Install Wiz...

thayden by Associate II
  • 7475 Views
  • 12 replies
  • 5 kudos

Error: No STM32 target found!

Hello, I’m still a complete beginner. I’m using an STM32WB55 board with the STM32CubeProgrammer. I’ve already flashed a few things onto the board, but currently, I can no longer connect to the board. Does anyone know how to fix this error?

error.PNG
Moritz18 by Associate II
  • 4274 Views
  • 9 replies
  • 2 kudos

Resolved! Crash when opening file

Hello,i just installed the most recent version of Cube Programmer but when i click the Open File tab and select a folder the program crashes immediately. I'm running it in Windows 11 64-bit on an Acer laptop, i selected the correct 64-bit version for...

omaroski by Associate II
  • 5575 Views
  • 7 replies
  • 1 kudos

Resolved! STM32Cube Programmer - invalid ELF-file

Hi folks,I have a Projekt on an STM32G431CBU. The programm runs without erros in DEBUG mode as well as in RELEASE Mode, when I flash it from the CubeIDE. For me this means the binaries are OK.But if I want to flash the ELF-Files to the MCU with Cube ...

CBerg by Senior II
  • 2763 Views
  • 3 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.