STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! STM32C031G4 recognized as STM32G03x/STM32G04x

Hi. I made a custom PCB with an STM32C031 microcontroller. However, I am unable to program it because it is recognized as 0x466. The problem occurs in both STMCubeProgrammer and the IDE. I checked 2 st-links with the latest firmware. Regards. 

Jin454_0-1724369266054.png
Jin454 by Associate III
  • 2721 Views
  • 5 replies
  • 5 kudos

Resolved! ST-Link/V2 CLI asking user to press return

This might have already been asked in the past, is there a way to not having to press return after programming a file with (old) ST-LINK CLI Utility?I am using the command line version which works fine but before the program runs ST-LINK stop and wai...

hans86 by Associate III
  • 3264 Views
  • 4 replies
  • 2 kudos

Resolved! No ST-LINK detected

No ST-LINK detected in STM32CubeProgrammer or the IDE. My ST-LINK/V2 ISOL shows up in Windows 11 Device Manger with driver 2.2.0.0 dated 2021-04-01. I thought the version on the ST website was 2.02? I was able to update it's firmware this morning. I ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.