2023-06-19 6:14 AM
Hi,
We are facing a issue to connect the ST link with our hardware setup ,,,, in today morning this is working fine but in afternoon facing the error in connection with the STlink debugger found error " Error: No STM32 Target found! If your product embeds Debug Authentication, please perform a discovery using debug Authentication."
Target voltage showing :- 0 or sometimes 0.22v (after refreshing)
Please suggest.
2023-06-19 7:23 AM
Hi,
0V from target: check voltage with dmm at your target, maybe it is really low.
You have any other target board, to check the st-link is working ok ?
2023-06-19 7:59 AM
Hello @Tajwar.Chandel
Try to switch to Power down Mode in ST Link Configuration.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-06-19 11:07 PM
Hi @Belaid,
Tried many times but still failed to connect.
2023-06-19 11:09 PM
Hello Ascha,
We have facing the same issue on 2 numbers of boards from yesterday afternoon.
Regards,
2023-06-20 12:12 AM
hi,
not connected under power down mode as well.
Regards,
2023-06-20 3:23 AM
>same issue on 2 numbers of boards from yesterday
so - you have many boards, and some working ok ?? or was it working before ?
2023-06-20 4:24 AM
Hi,
One more thing that this issue came after downgrade the firmware.
The MCU used STM32WB55RGV6.
Please suggest.
Regards,
Tajwar
2023-06-20 4:50 AM
Hi,
It was working before. 2 numbers boards down due to this issue.
We have 1 more board that is working ok.
Regards,
Tajwar
2023-12-20 11:27 PM
same problem with two boards and no resolve problem?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.