STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! Does Registers work in STM32Cube Programmer?

I am trying to use Registers in STM32CubeProgrammer to change the setting of GPIOB, but whenever I change a value. it just gets changes back to the value it had before! Is this because Registers is still in BETA or am I doing something wrong?

KMoel.1 by Associate II
  • 2348 Views
  • 7 replies
  • 0 kudos

Resolved! Did ST break SysTick in the last update? It used to work. Now it crashes because I think the interrupt vector is not set. Is this one of those known errors? How do I fix it?

When the SysTick interrupt fires the debugger quits. I cannot figure out where the NVIC_SetVector statement is for the SysTick. I think it is not set. But I can not find the vector table in the debugger to know for sure. This used to work, But when I...

KiptonM by Lead
  • 12468 Views
  • 30 replies
  • 0 kudos

STM32CubeProgrammer STM32G474 option bytes

Dear allI think the description is wrong or BOOT0/BOOT1 is swapped - see attachments.If the option bytes are programmed as shown under STM32CubeProgrammer.png, the controller boots from flash.Thanks in advance,Franz

FWege.1 by Associate III
  • 2330 Views
  • 1 replies
  • 1 kudos

Resolved! Write OTP lock bytes using ST-LINK/V2

Hi,i try to write the OTP area lock bytes using the ST-LINK/V2 programmer with the ST STM_Programmer_CLI tool included in the STM32CubeProgrammer software package.I can successfully write to the OTP area blocks using the -w32 command but if i try to ...

YWilk.1 by Associate II
  • 8706 Views
  • 17 replies
  • 0 kudos

Resolved! How do i need to create .bin file for an QSPI memory?

I am a beginner and I do according to this video "External Qaspi Loader How to - 05 - Qspi Driver Coding" https://youtu.be/XqCq0xtQmbI I uploaded the project "EXTERNAL QSPI Loader" to stm and now question about .bin fileHow to create a data file to b...

DK.7 by Senior
  • 3801 Views
  • 7 replies
  • 0 kudos

Resolved! STM32CubeProgrammer 2.10.0 and 2.11.0 External loader bug: if the EL's filename has more tha one dot (one dot only for its extension name) STM32CubeProgrammer goes in error.

If the name (filename) of module has more than one dot ( "." ) the STM32CubeProgrammer can list it in the external loder (EL) selection, but when STM32CubeProgrammer tries to use the module it fails (it generates an error).For example this EL name ge...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.