2022-07-11 5:44 AM
I've tried importing the examples into the IDE , complies fine but will not upload
- i get the "Failed to execute MI command:" error
if i use the stm32CubeProgrammer i can write to Flash(boot loader &program) but it never hands off to Qspi 0x90000000
i can make a small blinky program work out of the small boot flash -
so is it me ? the IDE ? a bad dev board?
(had successful projects utilizing f411' using the IDE )
possibly an explanation step by step like i'm 5years old ;) ?
2022-07-13 3:31 AM
Hello @RNevi.1 and welcome to the Community :),
It would be better to activate the gdb server log in your debug configuration (Debugger tab) and share it, this will help us to have more idea about the fails.
Make sure that you are using latest release of CubeIDE, Cubeprogrammer.
Try erasing the flash using Stm32Cubeporgrammer, this may solve your problem.
Imen
2022-07-13 5:18 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.