STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

In cubeprogrammer unbale to add start address

Hello,I am working on NUCLEO-H7 board . Its dual core CM7 and CM4. When I Erase the full flash then I click into erase and programming option but I unable to add start address . The core M7 is get programming , but in Core M4 i unable to do programmi...

0693W00000QMvVYQA1.png
MDeva.1 by Associate II
  • 4186 Views
  • 8 replies
  • 1 kudos

Not able to connect with stm32 cube programmer

Dear sir, I want to connect my stm32 board with stm32 cube programmer. ​but there is some issue, 1.i am able to read the device number , but the connect led does not turn green 2. Then I get messages of check boot configuration and serial port.3. I...

NSane.1 by Associate II
  • 3516 Views
  • 2 replies
  • 0 kudos

Resolved! Unable to run code STM32F411RET6

Hi,I'm unable to run code in my STM32F411RET6 when i'm running code, the debugger print :"Open On-Chip Debugger 0.11.0+dev-00449-g53fa0f7 (2022-06-09-09:40) Licensed under GNU GPL v2Info : Listening on port 6666 for tcl connectionsInfo : Listening on...

LBien.1 by Associate II
  • 4931 Views
  • 5 replies
  • 0 kudos

Why this error flashing STM32F746BGTx ?

I'm trying to flash a .bin file onto STM32F746BGTx  with CubeProgrammer 2.6.0.Yes , not latest but STM32F746 is not quite a new thing so I'd expect it to work.And get this:16:11:01 : File : vvvvv.bin 16:11:01 : Size : 1026247 Bytes 16:11:0...

Pavel A. by Super User
  • 1295 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.