STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! Extraction of bin file from microcontroller

Hey, sorry, I am pretty new to this. I have a rather basic question. I took apart a module that I have, within which there is STM32 microcontroller (part marking: STM32F103T8U77BA7E93PHL739). I want to know if it's possible to use the IDE to extract ...

BTay.1 by Associate II
  • 25037 Views
  • 30 replies
  • 1 kudos

Resolved! Issues with GDB Server...Need help!!

I have an STLINK-V3SET connected to a Seeed Lora-E5. I also have a Nucleo L476 developement board with on-board STLINK. On the Seeed board I am able to connect STM32CubeProgrammer and have loaded a file. I cannot connect however STM32CubeIDE as I get...

0693W00000QKIxAQAX.png 0693W00000QKIy3QAH.png
SWenn.1 by Senior III
  • 1478 Views
  • 2 replies
  • 0 kudos

Resolved! auto start SWV

Hi,the Serial wire viewer (SWV) has a command-line option. This only launch the viewer and the user has to press R to start.Is it possible to directly start the SWV?Or is there a shell trick for this? - Thomas*****************************************...

T B by Associate II
  • 2034 Views
  • 1 replies
  • 0 kudos

STM32G030K6T6 execute system memory bootloader, STM32CubeProgrammer connect ok, but can not program

Hi everyone, I use a JumpToBootloader( ) function in my code to execute system memory bootloader. and then STM32CubeProgrammer connect ok, but it can not program​MCU:STM32G030K6T6 STM32CubeProgrammer: v2.4.0Boot Interface: UART1 (PA9 PA10)+MAX13487EE...

0693W00000NsgxZQAR.png 0693W00000NsgxeQAB.png 0693W00000Nsgy3QAB.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.