STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! Peripheral in conflicts with others

Hello everyone, I have the following question: when, as in the attached image, you see a peripheral like the USART1 in yellow (in conflict with other peripherals), is it still possible to use it? I ask this information because I am looking for a NUCL...

SMusc.1 by Senior
  • 3889 Views
  • 17 replies
  • 7 kudos

ADC Scan Mode Problem

I would like to use ADC1_IN15 and ADC1_IN16 in STM32U073MCT6 for measuring voltage and current.However, it says that it is available if sequencer set to not fully configurable for Sequencer on parameter settings.I will do anything with sequencer. I a...

JamesMoriarty_0-1748951837410.png

Resolved! stm32cubemx usart code not generated for STM32F207ZGTx

The code for USART6 is not generated by STM32CubeMX tool for STM32F207ZGT6 MCU. I am trying to generate the baremetal code. I have created a default IOC file for this MCU, and configured USART6 as Ascychronous mode. After this I wanted to configure t...

Resolved! CubeMX use case

Last question. Can I use stm32cubeMX also for my project or is it better to continue with CUBE IDE?

SMusc.1 by Senior
  • 1194 Views
  • 1 replies
  • 0 kudos

where did lwIP go?

I cannot find the lwIP component for FreeRTOS in the latest STM32MX options.I installed the package FreeRTOS from the package install STMicroelectronics tab but lwIP is not available nor do I see and option to install the package.Can this be installe...

Resolved! SDDataLogFilex missing

I'm trying the example for STEVAL-STWINBX1 but when i use cubemx/cubeide example selector for STEVAL-STWINBX1, i only see 3 BLE and 1 NFC example but the SDDataLogFilex is missing.Is this normal ? How can i get the SDDataLogFilex example ?

nicolas by Senior II
  • 1168 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.