STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1762 Views
  • 0 replies
  • 2 kudos

Resolved! STM32F730Z8 USB failure with generated code

I just designed a board with the new STM32F730Z8 value line with embedded USB high speed PHY. I'm using a 16MHz external crystal and I am using the default code generated with CubeMX. It fails in the USBD_Init function. Following it through at first ...

bobert by Associate III
  • 1550 Views
  • 3 replies
  • 0 kudos

How to configure USB host MSC with CubeMX?

Hello, I use the STM32F767ZI card and I want to use USB OTG host communication. For that I tested the program provided by STM32CubeMX, "FatFs_USBDisk". The program worked well. But when I tried to redo the program using CubeMX. The p...

flor.5506 by Associate II
  • 4028 Views
  • 3 replies
  • 0 kudos

Setting up timers and toggling pins using CubeMx

Dear AllI am trying to use one of the timers on F303RE to toggle a pin at every count-up overflow event (let us say I need a jitter-free pulse). From CubeMx I get the impression that a GPIO pin can be associated with a timer and toggled by the event ...

Amir1 by Associate II
  • 5201 Views
  • 10 replies
  • 0 kudos

How to swap pins in STM32CubeMX v5?

Hi,I have a STM32F042F4Px. I would like to swap PA9/10 to PA11/12, but I'm having a hard time finding the option to do that in STM32CubeMX v5. This option still exists? Regards,Helder

Resolved! STM32CubeMX 5.1.0 RS485 Issue

Hiwith STM32CubeMX 5.1.0 on STM32F746BGTx there is an issue when I enable RS485.Cube doesn't genrate all funtions related to RS485, for example the main inizialization function HAL_RS485Ex_Init is not present in the code generated by Cuce.Attached th...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.