2019-03-06 6:46 AM
Hello,
I am working on a project for a STM32F767NIHx. I am using the STM32CubeMx tool and validating using RM0410. The problem I am having is that the i2c4_tx peripheral is not listed in dma1 stream5 on page 248 of the reference manual. CubeMx, however, gives dma1 stream5 as an option for the i2c4_tx. If I had to guess, I would say that the reference manual is wrong here and dma1 stream5 channel2 should actually be i2c4_tx instead of i2c4_rx, but I was wondering if someone could verify this for me.
Thank you very much for your assistance.
Solved! Go to Solution.
2019-03-08 7:44 AM
Hi @R
Thanks for the feedback.
You are right, i was able to reproduce the issue and it will be fixed in the next STM32CubeMX release.
Best Regards,
Nesrine.
2019-03-08 7:44 AM
Hi @R
Thanks for the feedback.
You are right, i was able to reproduce the issue and it will be fixed in the next STM32CubeMX release.
Best Regards,
Nesrine.
2019-03-08 7:54 AM
Thank you very much! I appreciate your time. Dma1 stream5 channel2 is for i2c4_rx- fair enough.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.