STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

What is the recommended alternative to using HAL?

The ST docs all refer me back to using HAL with CubeMX however I see many suggesting staying away from it.I could not find where to download and use libraries such as CMSIS for my STM32F407G Disco board Are the libraries I need already in my CubeIDE ...

LMorr.3 by Senior II
  • 10990 Views
  • 11 replies
  • 5 kudos

Plan to upgrade mbedTLS from v2.16.2 to v3.6.x?

Hi, The mbedTLS v3.6.x is LTS version and released for quite long time. Do you have plan to upgrade mbedTLS to v3.6.x with MX? If not, customer shall manually integrate/upgrade the mbedTLS to v3.6.x. Could you please give me a guideline to do that. T...

Leo2Ruan by Associate III
  • 530 Views
  • 2 replies
  • 0 kudos

CubeMX bug in generating ThreadX files for Cortex_M55

Hello, Using the latest CubeMX 6.15.0 I was generating ThreadX for Secure - Non Secure Project (for STM32N6 - Cortex_M55). This did not add file : "\Middlewares\ST\threadx\ports\cortex_M55\gnu\src\txe_thread_secure_stack_allocate.c" and so is not add...

Wrong file name for linker script

When generating code for Makefile, the MacOS version 6.15 succeeds while the Linux version 6.15 fails.I have the same version of firmware packages installed on both OS.MacOS STM32CubeMX produce this following snippet in the Makefile##################...

Resolved! How to set STM32H755 sysclk to 480MHz?

Hi there,According to the STM32H755 datasheet, the Cortex-M7 frequency can reach up to 480MHz.However, when I configure the sysclk in STM32CubeMX, it shows the maximum frequency is 300MHz.What's wrong with my config? Or is there any misunderstanding ...

Junde_0-1755251128177.png
Junde by Senior III
  • 2366 Views
  • 3 replies
  • 4 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.