STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! TouchGFX and X-CUBE-AI co-existence

Hi,I have a project with TouchGFX based on STM32N6570-DK.In STM32CubeMX, once I tried to add X-CUBE-AI, I got stuck, and the error is appeared as shown below.What does it mean?Once I removed the TouchGFX Graphic Application, the X-CUBE-AI can be enab...

ERROR_0-1756988586023.png
ERROR by Senior
  • 803 Views
  • 2 replies
  • 0 kudos

Resolved! STM32C092FCP6 SPI, SCK Pin remapping by CubeMX

Hello,when doing code generation by CubeMX, it seems, that there's no Pin-remapping done in certain cases, at STM32C092FCP6.In my case, I chose SPI2 in master full-duplex mode. SPI2_CLK is on PB8 at Pin1. A remapping from PB7 to PB8 has to be done by...

Screenshot 2025-09-04 155052.png
CBa by Associate
  • 541 Views
  • 1 replies
  • 1 kudos

Resolved! STM32CubeIDE PA3 Alternate Function Bug

Hi, There is a blatant bug in the STM32CubeIDE that has costed me a board iteration on a professional product. It says that pin PA3 is positive comparator input. When it isn't. Look here This is what the datasheet says.  

danielbathtub_0-1756991198601.png danielbathtub_1-1756991295544.png

STM32G0 minimum ADC frequency

I'm configuring an STM32G031, using the STM32CubeMX perspective in STM32CubeIDE.  I want to optimise for low power consumption.  My device uses the ADC and I see the ADC has a minimum acceptable frequency, 140kHz according to the data sheet (data she...

GrahamAU by Associate II
  • 1951 Views
  • 4 replies
  • 0 kudos

STM32H7xx ThreadX with HAL, bug in HAL_InitTick

function HAL_InitTick() in generated code from STM32Cube IDE does not register the TimeBase_TIM_PeriodElapsedCallback after HAL_TIM_Base_Start(&htim6). it just returns the result if Timer Start.setting up the callback is done after this but never rea...

weak attribute needed in app.freertos.c

in app_freertos.c, the hook prototypes are not all defined as __weak.  This requires either deleting those prototypes or rewriting them with the __weak attribute to avoid multiple definitions when they're actually used in user code.  I generally do n...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.