2025-08-11 4:39 PM
After updating to STM32CubeMX 6.15.0 with STM32CubeWBA FW V1.7.0 for the STM32WBA63CIUx, I noticed a change in how the HAL tick is driven.
In MX_APPE_Init() (generated in app_entry.c), CubeMX now creates a UTIL timer to increment the HAL tick:
/* Create an RTC based timer to trigger HAL tick increment */
UTIL_TIMER_Create(&TimerHALtick_Id,
HAL_TICK_FREQ_100HZ,
UTIL_TIMER_PERIODIC,
&TimerHALtickCB, 0);
uwTickFreq = HAL_TICK_FREQ_100HZ;
/* Start HAL tick timer */
UTIL_TIMER_StartWithPeriod(&TimerHALtick_Id, HAL_TICK_FREQ_100HZ);This runs at 100 Hz by default and causes my system to wake every 10 ms.
Previously, I used TIM17 for the HAL tick, with FreeRTOS (tickless idle) and STM32_WPAN BLE, and it worked well. Now, I see both TIM17 and this new UTIL timer, which leads to unnecessary wakeups.
My questions:
Is there official documentation on this new HAL tick implementation using UTIL_TIMER?
How can it be configured or disabled via STM32CubeMX instead of modifying the generated code?
If I want a 1 ms HAL tick, should I reconfigure the UTIL timer to 1000 Hz, or simply disable it and keep using TIM17?
What is the intended use case for this change in FW V1.7.0?
I could not find any CubeMX option to select between TIM17 and this UTIL timer. Any guidance or reference to documentation would be appreciated.
2025-08-12 2:29 AM
Hello @lgc
Could you please add the .ioc file you have createed.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-08-12 7:09 AM
Hello @STTwo-32, I attached the migrated .ioc file. Thank you.
2025-08-18 9:34 AM
Hello @STTwo-32 , is there an update on this topic?
Thanks and regards
2025-08-26 12:04 PM
Hello, just a friendly reminder about this topic. Is this being looked at by someone?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.