STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1762 Views
  • 0 replies
  • 2 kudos

CUBEMX Board Select: why not show dev board pinouts

Although I was quite excited to fire up the CUBEMX tool, ​I felt a little disappointed when, having selected on dev board (Nucleo etc), the tool did not then show me the mapping from the CPU pins to the board pins, with references to the on board LED...

Nor-Flash on Octospi1

I am using the eval board STM32L4R9I-EVAL.The generated code failde in OCTOSPI1_Init/ HAL_OSPI_AutoPolling:it runs by if ((hospi->State == HAL_OSPI_STATE_CMD_CFG) && (cfg->AutomaticStop == HAL_OSPI_AUTOMATIC_STOP_ENABLE)) {.....}else{..........}into...

Leo_Panda by Associate III
  • 6516 Views
  • 10 replies
  • 0 kudos

Resolved! How do I get L432KC SYSCLK to run at 80MHz?

Posted on October 11, 2017 at 17:26Hi,I have a L432KC Nucleo 32 and it never runs as fast as I expect it to.I have configured the clocks in STM32CubeMX as shown in my attached screenshot. I've configured MCO to match the SYSCLK so I can measure it w...

Cube FW 1.14 Seems Quite Broke

Hello:I loaded the newest Cube FW v1.14. On a project that generated and compiled perfectly well under 1.13, it now blows up in 1.14, with around 185 compile errors. Many related to including ARM include files that worked under 1.13 (arm_math.h)I hav...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.