STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1757 Views
  • 0 replies
  • 2 kudos

Resolved! TIM3 as Timebase Source on STM32F302RB

I recently switched an older project to CubeMX 5.1.0 and the F3 firmware package V1.10.0. We used freeRTOS and tim3 as the timebase source as tim1 and tim2 are already in use. The program does not pass the initial timebase configuration any more and ...

Blacbird by Associate II
  • 2373 Views
  • 4 replies
  • 0 kudos

Attempting to read/write to SD card via SDIO on STM32F

I'm trying to read and write to a microSD card using this reader from sparkfun https://www.sparkfun.com/products/12941 and a nucleo board with a STM32F429ZIT6U MCU via SDIO interface. I created the project through CubeMX V 4.21 (I used the most curre...

0690X000008AvtzQAC.png
RRayb by Associate II
  • 3932 Views
  • 5 replies
  • 0 kudos

Questions about 9-bit RS485 Multiprocessor Mode and HAL.

I am working on a project which is an upgrade of an existing project. The existing project was done with an Atmel processor, the current upgrade is based on an STM32F767. The project involves, among other things, multiple serial busses communicatin...

SBurc by Associate II
  • 3297 Views
  • 7 replies
  • 0 kudos

Is there any way to change "Vector Table base offset" and making it fixed rather than let Cube change it every time the code is regenerated?

Hello,I'm working with a bootloader so I need to change the Vector Table base offset to 0x00002000. This is done in system_stm32f1xx.c file:#define VECT_TAB_OFFSET 0x00002000U /*!< Vector Table base offset field. This value must be a multiple of 0x2...

CubeMX 5.1.0 Code Generation Warnings

Hi. I am using CubeMX code generation for the STM32F767VITx. I recently updated to CubeMX 5.1.0. Since updating, every time I choose to generate code, I get the following warning:" - These IPs still have some not configured or wrong parameter values:...

STM32H743ZI- NUCLEO rcc(clock) configuration

Hi, I use stm32h743zi nucleo board.I did clock configuration for stm32h7 with cubemx ,but I want to write clock configuration without hal library with registers.My clock configuration codes in attachment.Is there anyone who can tell me where is the m...

akaya by Associate II
  • 3543 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.