2019-04-24 2:35 PM
When doing complex Cube projects often you have to make decisions about peripherals or pins or I/O configurations for specific, but not always obvious, reasons. If nothing else it would be nice to be able to attach some notes to a project so someone using it down the road can figure out why you did what you did.
2019-04-24 3:10 PM
I often define custom symbols, because there's no other documented way to add custom info to a project.
These symbols, after code generation, become C #defines in main.h.
From there you can refer to them in other files.
Just some example....
#define EXT_UART 2 // use UART2 as external UART
#define EXT_UART_BAUDRATE 115200
#define HAS_BATTERY 1 // define if optional battery is assembled
-- pa
2019-04-25 10:39 AM
Thanks for your idea, that would work. It's too bad ST doesn't add a feature like that though -- you'd think it would be very easy to do. If they really wanted to make it more comprehensive they could let you document a specific item you chose to use or document a specific pin beyond just changing its name. But even just a blank page where you could write notes would be helpful.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.