STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1759 Views
  • 0 replies
  • 2 kudos

USB/CDC stops working by adding a asm("nop")

I have some problems with the USB/CDC communication. I have simplified the problem to the following:I'm using STM32CubeIDE and I've used CubeMX to configure a new project with STM32H743IIT6. I set up the clock and the USB/CDC device.The communication...

MRait.14 by Associate II
  • 6267 Views
  • 8 replies
  • 0 kudos

Need help with STM32L476RG SDIO + FATFS project

I have tried communication through SPI by following a lot of youtube tutorials. As there is no ready made library to take care of this through SPI, I decided to give SD mode a try. I am using the STM32L476RG microcontroller that has the SDMMC periphe...

KAbis.1 by Associate II
  • 3914 Views
  • 5 replies
  • 0 kudos

SDCard SDIO 4Bit with DMA using FatFs Q1: How to check if DMA is working? Q1: How to check if 4Bit Mode is set correctly?

Hi Community, I use a STM32F405 to access a uSDCard.Software: CubeMX V5.3 and SW4STM32 (Eclipse Neon.3 Release (4.6.3))The good news, I can communicate with the SDCard (create files, write content and delete files. So far so good, but now the questio...

0690X000009kCu9QAE.png
AWilk by Associate
  • 3325 Views
  • 4 replies
  • 2 kudos

I am using STM32F407 development board and I am trying to do flash read write operation but I am facing problem to erase a sector but am not able to do that.

Hi All,I am using STM32F407 development board and I am trying to do flash write operation but I am facing problem to erase a sector (I am using Sector no - 11 Block base addresses -0x080E 0000 - 0x080F FFFF size-128 Kbytes ) so that I can perform mul...

0693W000000VEdEQAW.png
Djain.1 by Associate II
  • 2309 Views
  • 3 replies
  • 0 kudos

Feature request : evalboard view

Hello, Currently cubeMx provides a pinout view usefull to see what is in use and to choose alternatesdepending of board layout constraints.Would it be possible to add an "eval board" view which would allow to see basically the same information but on...

0693W000000UtKGQA0.jpg
JulienD by Senior
  • 1641 Views
  • 3 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.