STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

How to power off D1 or D2 domain using CubeMX?

Board: Nucleo - H745ZI-QSw: Cube MX 5.6.0I want to use cube mx for generating simple blinky code (I use the board specific details), for some reason it doesn't work out, I suspect its because I cant specify how both cores will work together from MX. ...

sarojj7 by Associate III
  • 1393 Views
  • 1 replies
  • 0 kudos

CubeMX feature lost when integration with CubeIDE?

In the old standalone version of CubeMX one could access the datasheet/application notes appropriate to the board/CPU part your project was based on.Probably me being a bit dense but I can't see to find this in CubeIDE. Does an equivalent exist?Used ...

Resolved! Simulink freeze to open stm32cubeMx, possible cause... Java?

Hello,i'm Antonio and few week ago i've start to learn simulink and PIL simulation.I tring to test the IIR-Filter project from STM32_MAT-TARGET on my stm32f429i-DISK1 board with sw4stm32 toolchain but i've some problems ( used many time all the steps...

0693W000000Us1NQAS.png

Read file from USB flash drive with NUCLEO-F413ZH

Hi I would like to read a file on a USB stick. But phost-> gState remains HOST_ABORT_STATE; (usbh_core.c) . The code was generated with STM32CubeMX.USB_OTG_FS is set to Host_Only. Class for FS IP is set to Mass Storage Host Class in USB_HOST Mode and...

NDewe.2 by Associate II
  • 1704 Views
  • 2 replies
  • 0 kudos

Why STM32cubemx not generates header file

Hi everybody,I have installed STM32CUBEMX and also pack for F1 series(V 1.8).When i generate code for keil or truestudio i expect to have :#include "main.h"#include "stm32f1xx_hal1.h"inside of main.c file but unfortunately it does not generate #inclu...

AAhma.3 by Associate
  • 1107 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.