STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

May be a bug in STM32F3xx_HAL_Driver?

I'm creating serial communication application.I'm using STM32F303RE and USB CDC interface generated by STM32CubeMX.I used USBD_CDC_TransmitPacket() for transmitting data from device to PC.But when the data size == 64*x then read() in PC program didn'...

SAoya.1 by Associate
  • 1061 Views
  • 2 replies
  • 0 kudos

I installed STM32CubeMX 5.6.1. When I ran CubeMX it freezes when I click Install/Remove embedded software packages. How can I fix that?

EDIT:I installed STM32CubeMX 5.6.1. When I ran CubeMX it freezes when I click Install/Remove embedded software packages. How can I fix that? There is a section for managing software installation. When I click any button here ("CHECK FOR UPDATES" or "...

Why do I miss lib files even with update cubeMX?

Hi everyone,I created this small project.I uploaded package firmware to version 1.11.0 When I generate the code I have all these error messages.The only one we don't need to pay attention is the first error as it's a lib I imported myself.But why I h...

0693W000000X7fvQAC.png 0693W000000X7fqQAC.png 0693W000000X7flQAC.png
psvc.1 by Associate II
  • 3017 Views
  • 4 replies
  • 0 kudos

Partly Disabled Conflict Question from Noob

Sorry for these noob questions, but I am having a hard time understanding the exclamation marks in CubeMX. If somebody could please guide me here, it will be much appreciated.Example 1:The ADC converter is shown as Partially Disabled. However, I shou...

0693W000000WxM5QAK.jpg 0693W000000WxMAQA0.jpg 0693W000000WxMFQA0.jpg
JHenr.2 by Associate
  • 8474 Views
  • 2 replies
  • 3 kudos

UART driver missing in STM32CubeIDE.

I have generated my code using CubeMx tool in STM32CubeIDE. I find the stm32f4xx_hal_uart.c missing from the project. But when I generated the code by enabling the uart as asynchronous mode the second time, the uart appears in the driver folder. Why ...

0693W000000WSkkQAG.png
PKuma.51 by Associate II
  • 1554 Views
  • 2 replies
  • 0 kudos

Bug report: code generation STM32L475 IOT board

When I want to use the X-CUBE-BLE1.5.0.0 on STM32CubeMX, the file "b_l475e_iot01a1_bus.h/c" is not generated. Thus the project cannot be compiled.To reproduce:create new project on B-L475E-IOT01A boardoption of Targeted Language: C++Initialize all pe...

PADAM.1 by Associate III
  • 3911 Views
  • 9 replies
  • 1 kudos

Resolved! NRST stuck in reset_state

Hello,I am assigning pins on a STM32F446 micro in cubemx.I would like to give a pin name to NRST, but it is stuck in a reset_state, and won't let me change it. It is colored differently than other pins.Is it possible to change NRST, or does it stuck ...

0693W000000X8fSQAS.png
JAzri.1 by Associate
  • 1426 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.