2020-05-08 10:33 AM
Hello,
I am assigning pins on a STM32F446 micro in cubemx.
I would like to give a pin name to NRST, but it is stuck in a reset_state, and won't let me change it. It is colored differently than other pins.
Is it possible to change NRST, or does it stuck like that to signify that it is the reset pin? Still going to use it as the reset pin, but not sure if that has to be specified somehow.
I have the same exact issue with the BOOT0 pin. Is it possible to change the BOOT0 pin?
Solved! Go to Solution.
2020-05-08 10:58 AM
Perhaps look at a data sheet.
The NRST and BOOT0 pins are not assignable.
NRST will be stuck low if you failed to connect VDDA
2020-05-08 10:58 AM
Perhaps look at a data sheet.
The NRST and BOOT0 pins are not assignable.
NRST will be stuck low if you failed to connect VDDA
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.