STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

How do I program my STM32L4R9 with SDMMC and FatFS?

Hello,I would like to write a simple program for writing CSV files to a micro SD card on a custom board I made with my STM32L4R9. The card works on 3.3V and my STM on 1.8V, so I'm using a level shifter.For now, I selected SDMMC1 4 bits wide bus and F...

GMelo.2 by Associate II
  • 2577 Views
  • 5 replies
  • 0 kudos

Why does Stm32CubeMX not work.

The CPU is STM32L071KZ. I can select it in two packages. I pick it, assign pins, select a folder to store, select STM32Cube as IDE. It creates the code (ther eeven is an SRC and INC folder, but no .project. STM32Cube refuses to open it.I try TrueSTUD...

FVosm.1 by Associate
  • 781 Views
  • 1 replies
  • 0 kudos

I can't download stm32cubemx.

I want to download stm32cubemx.So I received the ST company's mail link.However, an error occurs in the link (404 NOT FOUND)What should I do? I need help.

Yoh.1 by Associate
  • 883 Views
  • 1 replies
  • 0 kudos

Keil throws errors after importing settings from CubeMX

I got to the point where keil opens a project using this manual https://www.keil.com/pack/doc/STM32Cube/General/html/cubemx_proj.htmland imports settings from CubeMx but writes the following errors:STM32G071RBT6 - Nucleo board (noBSP)LL triedHAL trie...

0690X00000DAHLDQA5.png
DKorz.1 by Associate
  • 993 Views
  • 1 replies
  • 0 kudos

Resolved! Multiple spi_nss pins?

I am assigning pins on a STM32F446 micro in cubemx, and I would like to connect multiple chips to the micro on one spi bus.I would like each chip to be connected to a separate chip select pin, aka spi_nss.When I try to assign a second spi_nss pin, it...

JAzri.1 by Associate
  • 2245 Views
  • 1 replies
  • 0 kudos

Resolved! Enable encoder mode on Ch3 & Ch4 of timer?

Hello,I am assigning pins on a STM32F446 micro in cubemx, and I would like to read 2 encoders.When selecting Encoder Mode under the Combined Channels dropdown of the timer configuration, it automatically selects ch1 & ch2.Ch1 of the timer conflicts w...

0693W000000X6q4QAC.png
JAzri.1 by Associate
  • 2897 Views
  • 1 replies
  • 0 kudos

Nucleo-L4A6ZG not supported in STM32CubeMX/IDE

I have Nucleo-L4A6ZG board and want to use STM32CubeIDE o program it, but there is no Nucleo-L4A6ZG board in the Board Selector list. Is there a package I can install for it or I must select STM32L4A6ZG in MCU Selector and configure the rest myself?

FVran.1 by Associate
  • 1750 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.