STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! Bug report: CubeMX on STM32WBA55CG with ThreadX

CubeMX version 6.16.1 I found STM32WBA55CG project with ThreadX,  the  parameter of "TX_LOW_POWER_USER_ENTER" and "TX_LOW_POWER_USER_EXIT" will be reset to default after the ioc re-open.This bug can be 100% reproduce. 

Kenwang by Associate III
  • 416 Views
  • 4 replies
  • 1 kudos

Generation of ports definition to main.h is inconvenient

Ports definition in main.h forced to include too mutch in dependend source files when one needs ports definition only.More convenient dedicated header file with ports definition only. Something like ports.h.It would be nice to have more layered struc...

vybor by Associate III
  • 404 Views
  • 4 replies
  • 3 kudos

Cannot set ITMENA

I'm attempting to follow https://community.st.com/t5/stm32-mcus/using-the-itm-console-for-printf-redirects-and-lwip-debug/tac-p/850072/highlight/true#M1661 but this always fails. This is on an STM32F303K8T. My reference manual saysand offers an examp...

avidroneg_0-1769105638276.png
avidroneg by Associate III
  • 293 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.