2023-12-18 4:34 PM - edited 2023-12-18 4:37 PM
On a Nucleo-H563ZI with CubeIDE 1.14.0 and firmware package for H5 1.1.1.
I managed to get SPI transmit and receive using DMA, triggered by a timer, going not using linked lists. I get my requested number of transmissions and results into my buffers as witnessed on an oscilloscope and a live watchpoint.
But when I enable circular mode, no other modifications, in MX_SPI1_Init - HAL_SPI_Init - HAL_SPI_MspInit it sets up
NodeConfig.Init.SrcDataWidth = DMA_SRC_DATAWIDTH_WORD;
NodeConfig.Init.DestDataWidth = DMA_DEST_DATAWIDTH_HALFWORD;
builds the node (whatever that is), inserts it into the correct DMA channel, sets circular mode, basically looks like magic but I can imagine what it is doing. But then the stuff in the NodeConfig doesn't get applied to handle_GPDMA1_Channel1, so later when I finally call HAL_SPI_TransmitReceive_DMA, it gets grumpy around line 2230 because hspi->hdmarx->Init is all zeros still. It never got updated maybe?
I think there is a problem with HAL_SPI_MspInit in stm32h5xx_hal_msp.c .
Thanks,
Andrei (from the Great (not very) White North)
2023-12-18 4:44 PM
2023-12-19 3:07 PM - edited 2023-12-19 3:26 PM
In HAL_SPI_MspInit (in spi.c with separate files for each peripheral or main.c without), the initialization of NodeConfig.Init looks correct, but there doesn't seem to be any code to transfer it from NodeConfig.Init into the Init member of the spiHandle passed into the function.
2024-05-12 4:09 PM
Were you able to solve this issue? I have been struggling to do something similar on the STMU5 MCU
2024-05-13 10:17 AM
I suppose I did.
SPI set up as a full-duplex master. With DMA for SPI TX set up as a standard request rather than a linked-list request, with trigger on TIM15 TRGO. SPI RX pretty much out of the box, peripheral to memory, source address increment disabled, destination enabled.
Transfers started using:
halStatus = HAL_SPI_TransmitReceive_DMA(&hspi1, (uint8_t*) &forceData, (uint8_t*) rawADCCounts,
NUMBER_OF_VALUES_TO_TRANCEIVE * 2);
And then call HAL_SPI_TransmitReceive_DMA again in HAL_SPI_TxRxCpltCallback, or else it will stop automatically after one request.
But I gave up on using linked-list mode. I seem to remember finding a YouTube video from the ST MOOC for the H5 that went over DMA and used standard mode. They never went into linked-list mode and I was more interested in getting ANYTHING working than chasing the linked-list bone.
A
2024-05-13 11:23 AM
Got it. Okay I was able to get something similar working in linked-list mode by using this function: __HAL_LINKDMA(&hspi1, hdmarx, handle_GPDMA1_Channel15);
2025-09-20 9:22 PM
2026-01-21 11:48 AM
Okay, I'd like to bring up this issue again.
Now Nucleo-H563ZI, CubeMX 5.16.1, CubeIDE 2.0.0, firmware package for H5 1.5.1.
As described in the original post, a call to HAL_SPI_TransmitReceive_DMA (see the previously attached project) always fails in the code:
/* Packing mode management is enabled by the DMA settings */
if (((hspi->Init.DataSize > SPI_DATASIZE_16BIT) && \
((hspi->hdmarx->Init.DestDataWidth != DMA_DEST_DATAWIDTH_WORD) || \
(hspi->hdmatx->Init.SrcDataWidth != DMA_SRC_DATAWIDTH_WORD)) && \
(IS_SPI_FULL_INSTANCE(hspi->Instance))) || \
((hspi->Init.DataSize > SPI_DATASIZE_8BIT) && \
((hspi->hdmarx->Init.DestDataWidth == DMA_DEST_DATAWIDTH_BYTE) || \
(hspi->hdmatx->Init.SrcDataWidth == DMA_SRC_DATAWIDTH_BYTE))))
{
/* Restriction the DMA data received is not allowed in this mode */
/* Unlock the process */
__HAL_UNLOCK(hspi);
return HAL_ERROR;
}because hspi->hdmarx->Init.DestDataWidth is 0, even though it is set up in HAL_SPI_MspInit to have:
NodeConfig.Init.SrcDataWidth = DMA_SRC_DATAWIDTH_WORD;So, somewhere in the initialization sequence, the NodeConfig structure is not being applied to the SPI handle.
Can I ask someone in ST support to take a look at this please?
2026-01-21 6:44 PM - edited 2026-01-21 6:47 PM
Do not use HAL_SPI_TransmitReceive_DMA().
"I am using Gemini for Korean-to-English translation. Please understand that there may be some unnatural phrasing."
2026-01-21 8:29 PM
Yeah, I even tried that code this morning. My SPI bus didn't start, and adding another layer of voodoo just rubbed me the wrong way. I've seen this same issue brought up thrice in these communities and ST even opened an issue on it in 2023. I'd like to see a proper example using HAL code before hacking registers. But thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.