STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! Generation code to CPP files

It is very inconvenient to have regenerated C files in C++ project.Problem is not main.c only, *_it.c as well. In C++ project one have to call methods of class from interrupt handlers.It is not possible to make directly from *_it.c. Indirect call cha...

vybor by Associate III
  • 913 Views
  • 10 replies
  • 9 kudos

Resolved! stm32f030cctx uart generated code bug

hello,now I am using stm32f030cct6 to design a simple program. i used all the 6 uarts of this chip. it works fine, but the interrupt code generated by STM32CubeMX has a simple bug. the code as below.for the uart6, there is a useless (&huart6);  i thi...

dqsh06_0-1769566375098.png
dqsh06 by Senior
  • 336 Views
  • 2 replies
  • 0 kudos

STM32N6 RIF and MMT autoconfiguration errors

Reporting two issues when using STM32CubeMX v6.16.1 to generate STM32N6 code. I created new secure only template project for STM32N6570-DK to demonstrate the issue (it's attached).Only changes to the new project are these:In MMT defined RAM2 area ove...

MikkLeini_2-1769067127587.png MikkLeini_1-1769067113592.png

Migrating STM32F469NIH6 to STM32F769NIH6

I'm considering migrating from STM32F469NIH6 to STM32F769NIH6. From data sheets it is apparant that these two MCU's have compatible pinout, however the pinout compatibility tool of STM32CUBEMX V6.15.0 doesn't show these MCU's as compatible, why is th...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.