STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! X-CUBE-ISP not found in STM32CubeMX

I'm using STM32CubeMX for STM32N657x0HxQ controller. I would like to use ST ISP Library to handle MB1854 camera module. But I could not find the X-CUBE-ISP in STM32CubeMX Pinout & Configuration page, which is as follows. So I tried to import x-cube-i...

스크린샷 2026-01-21 131702.png 스크린샷 2026-01-21 131949.png
JaeLee by Associate II
  • 447 Views
  • 3 replies
  • 0 kudos

Resolved! How to configure Downsize of DCMIPP pipe1 with STM32CubeMX

I'm using STM32N6570-DK board and developing an image processing application.When I tried to use STM32CubeMX to generate the project, I was able to set DCMIPP Pipe1 just like the attached screen capture.I would like to downsize the source image data ...

스크린샷 2026-01-20 103147.png
JaeLee by Associate II
  • 428 Views
  • 3 replies
  • 0 kudos

Resolved! STM32H7S7L8 usb HS and FS IRQ

Hello, I'm working with the STM32H7S7L8-DK and i want to use both USB HS and FS in device mode  but it seems in cube mx that i'm unable to enable both IRQ If i enable the HS one the FS one isn't generated and same fort the other way Is it a bug  and ...

Hamady by Senior
  • 836 Views
  • 8 replies
  • 1 kudos

Resolved! Unable to make LwIP work with FreeRTOS using CMSIS_V2

Hello!I have encountered a problem - I am unable to create a project for STM32F769I-DISCO board with both FreeRTOS using CMSIS_V2 interface and LwIP with NO_SYS parameter set to "OS Used".In old project that was setup with STM32CubeMX V6.14.0 using S...

FreeRTOS with CMSIS_V2 selected.png LWIP forces OS Not Used setting.png CubeMX 6.16.1.png
_AdamNtrx by Associate III
  • 770 Views
  • 7 replies
  • 2 kudos

SmartCard mode Parity is not initialized

When choosing SmartCard mode for USART, parameter Parity is automatically set to Even. However generated code in usart.c, does not has:hsmartcard1.Init.Parity = SMARTCARD_PARITY_EVEN;Only when I manually reselect that in GUI, the parity will be set i...

eSelix by Associate
  • 272 Views
  • 1 replies
  • 0 kudos

Resolved! cubeMX:access to example selector

When I open the official example using the example selector, CubeMX cannot display the graphical configuration of that example. I would like to know if it is possible to display the graphical configuration of the example in CubeMX. Thank you very muc...

stm64 by Associate II
  • 1059 Views
  • 16 replies
  • 5 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.