2026-01-27 12:33 AM
I select a new project and select the STM32L100C6U6A. STM32CubeMX says it has 4 kBytes of RAM.
I generate the project for EWARM.
But when I generate the project for EWARM it puts stm32l100xba_flash.icf file in the project and that files says RAM is 16384 bytes.
And the datasheet for STM32L100C6U6A says 4 kByte.
Is this a bug in STM32CubeMX?
My application still seems to run without errors. IAR reports 9511 bytes of readwrite data memory used.
Why does it still work? Is the datasheet wrong and this device is actually delivered with 16 kBytes RAM?
2026-01-27 12:38 AM - edited 2026-01-27 4:43 AM
Hello @MSipo
Your detailed explanation is much appreciated.
Issue has been escalated to the dedicated team under internal ticket number 226018 for further analysis and resolution.
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-01-29 12:34 AM
How can I track this ticket number? How do I get an explanation?
We have a finished product where this could become a problem as we use too much RAM (9511 bytes), but our testing has not showed any errors in function.
In an older thread I posted about a similar bug for STM32G030F6P6 flash and got a ticket number and never received any follow up information if it was ever fixed.https://community.st.com/t5/stm32cubemx-mcus/stm32g030f6p6-says-32kbytes-flash-but-linker-script-says-64kbyte/m-p/599015#M26215
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.