2026-01-22 8:45 AM
The STM32N6 reference manual shows that IC18 drives the CSI2Host and CSIPHY IP blocks at a maximum frequency of 200 MHz. CubeMX generates this clock configuration code but does not show the clock path in the clock configuration window. Additionally, it does not provide any error checking and will allow IC18 to be configured above 200 MHz.
Clock tree diagram:
Maximum clock rate spec:
CubeMX generated code in HAL_DCMIPP_MspInit:
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_DCMIPP|RCC_PERIPHCLK_CSI;
PeriphClkInitStruct.DcmippClockSelection = RCC_DCMIPPCLKSOURCE_IC17;
PeriphClkInitStruct.ICSelection[RCC_IC17].ClockSelection = RCC_ICCLKSOURCE_PLL4;
PeriphClkInitStruct.ICSelection[RCC_IC17].ClockDivider = 1;
PeriphClkInitStruct.ICSelection[RCC_IC18].ClockSelection = RCC_ICCLKSOURCE_PLL4;
PeriphClkInitStruct.ICSelection[RCC_IC18].ClockDivider = 2;
2026-01-22 10:24 PM
Hello @xJIomqygrecz
I'm currently checking this behavior. I will get back to you asap.
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-01-28 4:28 PM
@Ghofrane GSOURI, were you able to confirm this bug?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.