2022-07-31 10:27 AM
I need to use FreeRTOS 10.4.6 in order to use SystemView. Therefore, I downloaded the new FreeRTOS version and replaced the relevant files in the repository file. However, the "Tool Code Generation" generates a FreeRTOSConfig.h with the old version. I replaced the FreeRTOSConfig.h manually with a file from the demo project. Applying the "Tool Code Generation" replaces the Config file with the old FreeRTOS version. How can I make sure a proper config file exists for my project? "Tool Code Generation" might be applied several times.
2022-08-15 5:29 AM
Hi JMA,
CubeMX is integrated into CubeIDE and manages the "code generation".
One version of CubeMX (integrated into CubeIDE) is only shipping one version of FreeRTOS.
CubeMX is awesome for prototyping and moving fast. But when you move from prototype to application code development and want full control over all the software components, then the CDT project type is a more sustainable project format!
If you want to control which versions of a specific middleware that you rely on, then I would not rely on CubeMX to generate that code.
Feel free to share additional questions/feedback.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.