STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! MODBUS communication using STM32F730

I'm trying to use STM32F730 for MODBUS communication. The datasheet and reference manual both shows support for MODBUS. However the problem is :when i use cubemx for configuration purpose it generated following message "This peripheral has no paramet...

NSing.5 by Senior
  • 7352 Views
  • 8 replies
  • 0 kudos

LL_USART_Init generated by CubeMX size reduction ?

Hi everyone,Like most of embedded work, our project aims to have the smallest size possible.Looking at what I can optimize, I came across the LL_USART_Init function that is generated by CubeMx.This function uses LL_USART-SetBaudRate which needs to us...

WGend.15 by Associate III
  • 1387 Views
  • 1 replies
  • 0 kudos

Resolved! CubeMX 6.7 Removes Power Regulator Voltage Scale?

I have a project with an STM32H745. After I opened it with CubeMX 6.7 and migrated the project I noticed there were many errors in the clock configuration. I recognized these errors as relating the the Voltage Scale setting. I noticed it was missin...

0693W00000Y7VJOQA3.png 0693W00000Y7VJYQA3.png

Resolved! Only half the adcs channel manage to read their pins correctly

So, we are using ADCs on the STM32h743XIH6 rev V to read DC and low-frequency signals. We noticed we have half the ADC channels working correctly and half not working correctly. Those working correctly are:ADC3P1 PC3_CADC2P1 PA1_CADC3P0 PC2_CADC3P2 P...

DLuss.1 by Associate II
  • 1917 Views
  • 3 replies
  • 0 kudos

LL ADC with DMA

I have problem with configuration ADC (6 regular channel) and DMA. CubeMX generate next code:static void MX_ADC_Init(void) { ... /** Configure Regular Channel */ LL_ADC_REG_SetSequencerChAdd(ADC1, LL_ADC_PATH_INTERNAL_VREFINT); /** Configure ...

0690X0000088R48QAE.png
IByco by Associate
  • 1656 Views
  • 1 replies
  • 3 kudos

Automatic upgrade of STM32H7_ETH_Example_IDE1.6.1 LWIP/FREERTOS by STM32CubeMx V6.2.1/FW_H7_V1.9.0 to V6.6.1/FW_H7_V1.10.0 breaks the example.

I am able to run the example STM32H7_ETH_Example_IDE1.6.1 properly.This is a basic LWIP/FREERTOS example implementing ping on fixed IP.I recreated the example in minute detail in STM32CubeMX V6.6.1 FW_H71.10.0; it failed.In the process of finding the...

Johi by Senior III
  • 2594 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.