STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

bug in HAL_UART_Transmit_DMA

I wrote an application configuring the USART for DMA transmission. The first call to HAL_UART_Transmit_DMA works correctly and the expected bytes are sent. However, every subsequent call fails with HAL_UART_STATE_BUSY.It appears that the uart state i...

MScha.8 by Associate II
  • 3678 Views
  • 4 replies
  • 0 kudos

STM32CubeMx warning when using 4 UARTs

Dear allI'm using STM32G070KBT in my product, as it has 4 UARTs.I want to use the 4 UARTs in asynchronous mode, no HW control, UARTs 1 and 2 use RX/TX, while UARTs 3 and 4 use only RX.When defining all those UARTs in STM32CubeMx, I've some warnings t...

jerome2 by Associate II
  • 3924 Views
  • 6 replies
  • 0 kudos

Resolved! CubeMX Generated Code: Build Option Greyed Out

Hello,I am using the NUCLEO-F401RE with the NUCLEO-IDB05A2 bluetooth low energy expansion board. I am trying to run the sample demo code that is part of the X-CUBE-BLE1 software package (SensorDemoBLE). I followed the instructions in this video below...

0693W00000Y7P7WQAV.png
KMew by Senior III
  • 4164 Views
  • 2 replies
  • 0 kudos

Resolved! RTC losing fractions of second on uP reset - how to solve?

My code initialises the RTC using the standard CubeMX code but before setting the clock it tests for a valid year > 2018. This works perfectly and the time and date are preserved through resets of the uP. However, it appear that either the reset or t...

STM32L073- multiple USB device interfaces

Hello,We are currently evaluating the STM32L073 series in terms of the possibility to configure the USB device as either:3x interfaces, all serial (COM) ports.3x interfaces, 2x serial (COM) port and 1x mass storage device.In the STM32 studio I have n...

0693W00000WL5f5QAD.png

Resolved! How to speed up STM32G474 float number calculation?

Hello,I am new to STM32 MCU and right now using a 170MHz STM32G474 MCU for my project. I did a test today and found out the float number calculation speed of the MCU is quite slow.It takes 6.3us to finish the calculation in Fig.1. (I set a GPIO pin h...

0693W00000Y7RFXQA3.png 0693W00000Y7RFmQAN.png 0693W00000Y7RG1QAN.png
QMa.1 by Associate
  • 5293 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.