2022-12-08 6:39 AM
So, we are using ADCs on the STM32h743XIH6 rev V to read DC and low-frequency signals. We noticed we have half the ADC channels working correctly and half not working correctly. Those working correctly are:
ADC3P1 PC3_C
ADC2P1 PA1_C
ADC3P0 PC2_C
ADC3P2 PF9
ADC2P4 PC4
ADC2P0 PA0_C
and those not working are
ADC1P12 PC2
ADC2P5 PB1
ADC2P10 PC0
ADC1P2 PF11
ADC1P3 PA6
ADC3P3 PF7
ADC3P4 PF5
Note that we switched the signals from ADC1 to ADC2 on the signals not working and still would not read correct values. We are reading varying signals (even with dc signal in) with usually a low value around 0x9ff or 0x9df (on 16 bits reading). Good signals keep working when changing ADC too. The pins are working both in GPIO output and input correclty so we do not think it is a solder issue. We also probed the signal right by the processor and it stays clean.
Any idea what the problem could be? We ran out of ideas.
Solved! Go to Solution.
2022-12-09 8:38 AM
Issue was with the Low-level driver generated by CubeMx, Switching to HAL cubeMx code generation solved the issue (with our user code interacting with adc staying LL).
note: GPIO, ADC and RCC (not sure this one matters, the other 2 for sure) drivers had to be changed to HAL
2022-12-09 8:38 AM
Issue was with the Low-level driver generated by CubeMx, Switching to HAL cubeMx code generation solved the issue (with our user code interacting with adc staying LL).
note: GPIO, ADC and RCC (not sure this one matters, the other 2 for sure) drivers had to be changed to HAL
2023-01-04 2:45 AM
Hi @DLuss.1 ,
Glad to know that your issue is already resolved.
But it will be helpful for us if you can share your .ioc file that can help us to reproduce the issue.
We need to deeply analyze it to identify the root cause: STM32CubeMX or the LL driver?
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-01-04 5:50 AM
It is attached in the online support Case Number 00169037
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.