STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! Cubemx & Stm32U031

Inside Cube config, i do not get the other internal connected pins on pin 14, only PA8... in older versions it was available. The chip is STM32U031F8... What do i do wrong.. i need to use the uart_tx function on pin 14... Thank you  Old version from ...

KJeps3_0-1771255803170.jpeg KJeps3_1-1771255810598.jpeg
KJeps.3 by Associate III
  • 514 Views
  • 5 replies
  • 1 kudos

Resolved! STM32CubeMX generated USBPD not compiling

Hello, I created a complex project for a STM32H573 based custom board. That project is ThreadX based and it shall use the USPBD package. I generated to project with STM32CubeMX version 6.16.1 using STM32Cube MCU Package for STM32H5 Series 1.5.1 (see ...

TThan by Associate III
  • 556 Views
  • 4 replies
  • 3 kudos

Where to report bugs?

I've reported a STM32CubeMX bug, but I am afraid that there is no one to look at it. Is there any better place to report bugs/issues? Things I've reported are quite a blocker for me and I really need to know if there is anyone working on it, or I'll ...

Resolved! Can CubeMX generate a cpp file

I'm using "STM32CubeIDE for Visual Studio Code" on Ubuntu 22.04.  I have a situation where I'm making a driver for a chip where it very much benefits me to make the driver into a class and instantiate several instances of it.Generally speaking, what ...

sethkaz by Associate III
  • 405 Views
  • 2 replies
  • 3 kudos

ThreadX or FreeRTOS with FileX?

Hi,This is for STM32U5 and STM32H7 series MCUs.I was starting to use ThreadX because it looked like it was preferred over FreeRTOS. Now it looks like it is going the other way FreeRTOS is preferred over ThreadX ... or so I read/watched.I liked Thread...

Rodo by Senior
  • 982 Views
  • 3 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.