STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! STM32CubeMX 6.16.0 – Fixed Nominal CAN Bit Timing Values

Hello,I’ve noticed a difference in behavior between STM32CubeMX configurations for STM32H7 and STM32N6 series.On STM32H7, when configuring CAN bit timing, the parameters such as Nominal Time Quantum, Nominal Time for one bit, and Nominal Baud Rate up...

Duc_0-1770995533811.png
Duc by Senior
  • 596 Views
  • 5 replies
  • 2 kudos

Using SPI DMA at 16bit, dosent work on STM32H5

Hi. ST There is an error in the code that is generated by CubeMx when you use 16bit in SPI DMA transfer. Can be solved in the stm32h5xx_hal_msp.c file: /* USER CODE BEGIN SPI4_MspInit 1 */ memcpy(&handle_GPDMA1_Channel1.Init,&NodeConfig.Init, sizeof(...

spa23 by Associate III
  • 2214 Views
  • 4 replies
  • 2 kudos

Resolved! How to configure HSEM in STM32CubeMX

The HSEM option is not found in "System Core" in STM32CubeMX (version 6.15), and the configuration option for HSEM interrupt is only found in NVIC. How to configure HSEM in STM32CubeMX. When I selected the LL library environment, the generated source...

Snipaste_2025-11-07_15-12-55.png
liuxw by Associate II
  • 1355 Views
  • 6 replies
  • 4 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.