STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! CubeMX 6.16.1 linker generation bugs

Hello, We appear to be experiencing a severe code generation bug with CubeMX. After naming and sizing application regions in the memory management tool, what used to generate a correct linker script now generates bad output.Upon generation the linker...

sandwizard_0-1767430692804.png

Resolved! CMAKE project generates unsuppressable macro redefine

I am using cubemx to generate a CMAKE project for a NUCLEO_144 based board (NUCLEO_H563).Project generation creates a cmake/stm32cubemx/CmakeLists.txt file that generates a macro define "USE_NUCLEO_144".it also auto creates a stm32h5xx_nucleo_conf.h ...

Resolved! CubeMx issue: fixed FDCAN Tx buffer allocation = 32

Split from this thread. Yes, but No!CubeMX V6.16 now allows only exactly 32 TX Buffers ((TX Buffer Nbr + TX Fifo Queue Elmts Nbr) == 32).But less then 32 TX Buffer is allows by the Hardware, and some times, required if You want to maximize the RX Buf...

MHoll.2 by Senior III
  • 731 Views
  • 2 replies
  • 1 kudos

Resolved! CubeMX fails to load IOC file after enabling RAMCFG

There's a bug in latest STM32CubeMX v6.16.1. When enabling RAMCFG for Appli on STM32N6 MCU, the IOC file becomes unloadable.I attached the demonstration IOC file. I created new project for STM32N6570-DK board, enabled RAMCFG peripheral for Appli, che...

MikkLeini_0-1769065922714.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.