STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! Multiple ADCs and GPIOs

Hi, I am trying to set 4 ADC in single-ended modes with a minimum of 26 GPIOs which will be used in inputs or outputs, the thing is I have a lot of conflict with the ADC. I have the yellow warning sign even if there are all green is that an issue eve...

Vueko by Associate III
  • 1684 Views
  • 2 replies
  • 0 kudos

Resolved! Documentation about settings in CubeMX?

Hello, I'd like to better understand some settings in CubeMX to be sure default settings are OK for my application.Starting with USART2 Configuration for example:- in "DMA Settings" tab, what behavior is modified by the Priority dropdown (Low, Medium...

Thomas LB by Associate III
  • 4666 Views
  • 6 replies
  • 3 kudos

cubemx 6.3.0,STM32L562VETx,sd+FATFS,BSP code for SD

    Nothing generated by CubeMx: the BSP code has to be added to the project according to the board (ST or custom) in use.   ​Does this MCU need to manually transplant the BSP of SD card?Why did the F103 and f429 MCU have the corresponding BSP code f...

0693W00000D1iYIQAZ.jpg 0693W00000D1iXEQAZ.jpg
MShao.1 by Associate III
  • 2165 Views
  • 2 replies
  • 2 kudos

Can not execute f_open

I have connected microsd by SDIo to STM4Disc1 board. I am using SD 4 bit.  I see on STM forums there is a bug and needs to set 1bit in MX_SDIO_SD_Initso I changed to   hsd.Init.BusWide = SDIO_BUS_WIDE_1B and reduce SDIO CLK by 192 factor.I am able to...

Nico3 by Senior
  • 1853 Views
  • 3 replies
  • 0 kudos

Problem with IDE

Hello, I've got problem with STMCubeIDE. You can see my problem at photos I attached. Can anyone help me to solve this problem. I try to work on Lenovo Legion 5 with Ryzen 5 5600h and RTX3060. Second graphic card is integrated with Ryzen CPU. This pr...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.