2023-07-08 10:04 AM
Hello,
I've got problem with STMCubeIDE. You can see my problem at photos I attached. Can anyone help me to solve this problem. I try to work on Lenovo Legion 5 with Ryzen 5 5600h and RTX3060. Second graphic card is integrated with Ryzen CPU.
This problem is at lot of windows at MX section when I try to configure my STM. I try to open this program with both graphic cards. I have latest drivers to both graphic cards. Try to standalone MX software but still same result.
Maybe someone had similar problem.
2023-07-10 2:17 AM
Hello @Grzesi3k777
First let me thank you for posting.
To be able to further investigate the issue, I will need you to provide:
BR,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-07-10 10:48 PM
Hello Semer,
thank you for your answer. For now I cannot answer to all your question but:
1. I am using Windows 11
2. STM CubeIDE I am using the latest version
3. Do you really need my IOC file? There is nothing for now because I create it for test to show the problem.
I don't have logs for now. You have to know that I tried CubeIDE at another computer with Windows 11 and I don't have this problem so it is not problem with OS. Maybe something in my computer maybe some drivers or something. I hope that you can help me with this topic.
2023-07-10 11:29 PM - edited 2023-07-10 11:30 PM
hi,
i have also a problem (on win PC ) when opening MX/ioc view - window is in pure white .
(this strange problem was suddenly beginning some month ago)
but closing this MX window and open again (just click on ioc file) starts it correct. so did you try this ?
2023-07-10 11:55 PM
Hi,
I didn't try it. So I have to try to reopen ioc file. I have to back home to test it so I'll let you know later.
2023-07-11 11:01 AM
Hi,
I tried your suggestion and unfortunatelly still have a problem. I reopen ioc file and still have this weird problem.
2023-07-13 10:17 PM
Do you maybe have any new suggestion how to solve this weird problem?
2023-07-17 10:19 PM
Hi,
How can I make this log file for you?
2023-08-07 1:31 PM
Hello,
Can anyone help me with this weird problem?
2023-08-11 2:43 AM
Hi @Grzesi3k777 ,
Sorry for such inconvenience.
I'm not sure it can provide you a workaround, but could you please have a look to this post that seems
similar to your case and where an update of the Windows display setting (probably talking about font size and
display scaling) helped :
https://community.st.com/t5/stm32cubemx-mcu/my-cubemx-ui-is-messed-up/m-p/571509/highlight/true#M25330
Let me know if that could work for you too.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.