STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

stm32cubemx fails to download packages

stm32cubemx fails to download packages due to inability to authorize at "myST->login".According to the crash dump it has happend because of jxbrowser plugin-7.30.2 (chomium version 108.0.5359.215).All extended attributes had been cleared (not trusted...

Screen Shot 2023-07-27 at 11.43.58 AM.png

Bug --- but EWARM V8.32project generation have a problem.

Using STM32CubeMX version 6.2.1.1) Create a project using STM32H755ZI, I named the project CubeMXError.2) Generate code.3) Open code with IAR, version 8.50.6.4) In IAR, right click in the workspace to adjust options for node "CubeMXError".5) In ...

GHolc.1 by Associate III
  • 2750 Views
  • 3 replies
  • 0 kudos

Resolved! Generate Report via command line

Hello everyone.Is there a way to generate the report files (pdf and txt) via command line in CubeMX?I run STM32CubeMX in command-line mode getting commands from a script,but I didn't find any commands about report generation in the command line summa...

nickf by Associate
  • 1353 Views
  • 1 replies
  • 0 kudos

usb cdc doesn’t work on stm32l152

I enabled usb cdc by stm32cubemx in an empty project. I connected dp, dm, gnd and (to ground). I tried a 1.5k pull up resistor on dp pin. But still I get “usb not recognized”. I am using stm32l152re-nucleo board.I have set up usb cdc on other stm boa...

Femah by Associate
  • 1713 Views
  • 2 replies
  • 0 kudos

configUSE_TASK_NOTIFICATIONS

you have to put "#define configUSE_TASK_NOTIFICATIONS 1" into FreeRTOSConfig.h to make notification to work.Even cube has enabled the funktion. Cube removes the line every time its saves the project.  

Resolved! octospi configuration cubemx

I have octospi hyperram memory to use on stm32h7b0 with nor flash I usually use stm32cubemx because it make the life easier but it's my first time configuring memories with it..can anyone help me with that ?

JJuli.1 by Associate II
  • 7505 Views
  • 10 replies
  • 1 kudos

Resolved! STM32U5 invalid SMPS warning during code generation

STM32CubeIDE 1.13.2 is showing a warning about SMPS for STM32U5 chips every time the code is generated (see attached).This is done even for chips which do not have the SMPS pinout, e.g. STM32U595VJT (non Q), which is completely invalid.But even when ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.