STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! STM32CudeMX base code generates a larger program file

Hi I made a program for STM32F103RG using STM32CubeMX and STM32CubeIDE a few years ago. The program is using the USB Device Mass storage software pack. I thought that I should update it with the latest version of it and made a new project since the o...

Resolved! STM32F746: ADC3 does not work with external trigger from timer

Hi,I made project that samples audio signals from the ADC at a constant rate. The trigger signal for the ADC conversion is generated by a timer. Now here's the thing:The code works fine on my STM32L432 Nucleo, STM32L4R5 Nucleo and STM32F429 Disco, bu...

SFahr by Associate III
  • 4925 Views
  • 8 replies
  • 0 kudos

Resolved! How to change HAL firmware version in STM32CubeIDE

Is it possible to revert a project to an earlier firmware version? I was able to upgrade, but now I can't figure out how to change back to the previous version.I also can't create a new project with the older firmware version either (the dropdown is ...

0693W000002liS6QAI.png 0693W000002liS1QAI.png
Miles1 by Associate III
  • 9451 Views
  • 6 replies
  • 0 kudos

Resolved! CubeMX injects LL_RTC_TAMPER_MASK_TAMPER1 for RTC Tamper 2

Hi, Just to notify a bug  :CubeMX injects LL_RTC_TAMPER_MASK_TAMPER1 for RTC Tamper 2 when generating codeSTM32CubeMX - STM32 Device Configuration Tool Version: 6.8.1-RC4STMCube FW_L0 V1.12.2 /** Enable the RTC Tamper 2*/LL_RTC_TAMPER_Enable(RTC, LL_...

Rla by Associate
  • 1736 Views
  • 2 replies
  • 0 kudos

STM32CubeMX 6.10.0 limit source frequency for ADC

I am trying to configure ADC for STM32H562VGT in STM32CubeMX but it is limiting maximum source frequency for ADC. It limits it to 75MHz (which is maximum frequency of ADC clock) but ADC clock has its internal divider.For example I want to use 120MHz ...

BlazejKrysztofiak_0-1700830415601.png

I2C MASTER TRANSMIT IS NOT WORKING

 STM32 DevloperBord : STM32F030C6T6TRCubeMX : version 6.7.0keil : version 5i2c config at standard mode I2C_Speed_Frequancy-100KHZ/*************************************************************************************/static void MX_I2C1_Init(void){/* ...

Hito by Associate II
  • 3148 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.