2023-11-25 1:40 AM
I can not open my project after update cubeMX to latest version.
Solved! Go to Solution.
2023-11-28 2:30 AM
Hello @nimaltd
After verification I was able to see the error.
The case was escalated internally for analysis and fix 167308 (this is an internal ticket number).
In the meanwhile, you can use the pack creator from the CubeMX 6.9.2 as a temporary solution.
KR,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-11-25 6:44 AM
Why not? What happens when you try?
2023-11-25 6:50 AM - edited 2023-11-25 6:52 AM
cubeMx works well. only packet generator does not work. nothing happen. only wait after open project.
2023-11-27 1:56 AM
I have tried with 2 pc. Both of them have the same problem.
2023-11-28 1:32 AM
Hello @nimaltd
First let me thank you for posting.
Could you describe the scenario which show this behavior.
Could you share the Cubemx log for that you can start the tool with command line.
KR,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-11-28 1:49 AM
Hello. This is not cubeMx error. Only in Stm32packCreator.
I can not open my previes project and can not use https://github.com/nimaltd/STM32-PACK/blob/main/SPIF/NimaLTD.I-CUBE-SPIF.2.0.1.pack for create a new project.
It was generated before update cubemx.
2023-11-28 2:30 AM
Hello @nimaltd
After verification I was able to see the error.
The case was escalated internally for analysis and fix 167308 (this is an internal ticket number).
In the meanwhile, you can use the pack creator from the CubeMX 6.9.2 as a temporary solution.
KR,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.