STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! Delay issues on HAL_SPI libraries

Hello everyone,  I am using SPI to communicate two Nucleo Boards (a NUCLEO-L432KC and a NUCLEO-F411RE one), and i found out a weird behavior. The idea was to perform a transaction Master -> Slave in order to select a "register" to read. Once the Slav...

vicfer89 by Associate II
  • 3783 Views
  • 5 replies
  • 0 kudos

Is a STM32CubeMX file available for Arduino Portenta H7

Hello,has someone created a complete definition of the "Arduino Portenta H7" board including the clocks in STM32CubeMX?I would like to use this board to develop and test some parts of projects.The creation of the IOC file is a lot of work that I want...

STM32U5 IAP_main example NOT working

Hi,I am using STM32CubeMX version 6.11.0 .I want to test the "IAP_main" example for the STM32U575I-EV.I start the project as follows : Then when I try to Generate Code for the STM32CubeIDE in CubeMX the following error occurs: The code gets generated...

IAP_main_u5_error0.png IAP_main_u5_error1.png IAP_main_u5_error2.png

Resolved! STM32U585QII6Q ADC4 Channels

Hello,I'm encountering an issue with STM32CubeMX while configuring the STM32U585QII6Q microcontroller. Specifically, when attempting to configure PD11 to ADC4_IN15, I find that the ADC4 channels are grayed out or inactive.While using STM32CubeMX, I c...

ari_v2 by Senior
  • 1949 Views
  • 2 replies
  • 0 kudos

Resolved! NUCLEO-H563ZI SPI Master example is not working

Hi I'm trying to run SPI_FullDuplex_ComIT_Master and Slave examples that use SPI1 on NUCLEO-H563ZI boards.The pin connections in the read me seems to be inaccurate i.e1. There is no PA5 on 10th pin of CN6 on the Nucleo but it is there on CN7.2. There...

WCarey_0-1712129354068.png
WCarey by Associate III
  • 2269 Views
  • 4 replies
  • 0 kudos

Resolved! STM32H750B-DK setup the BSP folder through the .ioc file

Hi,I am following a course (for a different STM board) to use the LCD touchscreen of the STM32H750B-DK board. In the course, they have added a BSP folder to their project which includes files such as are seen here: STMicroelectronics/stm32h750b-dk-bs...

Bxy by Associate II
  • 2678 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.