2024-03-26 2:03 AM
Hi,
I use several LD files in the project, depending on the selected build. After updating CubeMX (6.11.0) and CubeIDE (1.15.0), the default LD file appears in the project every time I generate code from CubeMX. Worst of all, all links to my LD files are removed. Each time I have to laboriously edit the project settings. Nightmare. Do you have that too?
Regards.
2024-04-01 1:27 AM
Hello @Maciej Frankowski
I would appreciate it if you could give me the project where you encountered the issue or at least provide me with the steps that I need to follow to reproduce it.
Also is this issue consistently reproduced?
I will be waiting for your feedback.
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-04-03 3:23 AM
Hello again @Maciej Frankowski
Thank you for your contributions and for your detailed explanations,
I confirm the issue on my side, it has been reported to STM32CubeMX development team .
Internal ticket number: 178127 (This is an internal tracking number and is not accessible or usable by customers).
I will keep you posted with updates.
Regards,
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-04-03 4:03 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.