2024-04-01 7:03 PM
I'm using CubeMX v6.11.0 to generate code for STM32G474.
When I change TIM20's "Request Number" from the default 1 to 4 and press "CTRL + S" to save or click "GENERATE CODE", the number always changes back to 1 automatically.
2024-04-01 11:55 PM
Hello @WZHWZH and welcome to the ST Community :smiling_face_with_smiling_eyes:.
Can you share your .ioc file.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-04-03 11:14 PM
It's already attached in the first post :)
2024-04-04 1:30 AM
Hello,
I've been able to set the Request number to 4 then saving the project. After closing and reopening again, everything works fine on my side (Request number is kept on 4):
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-04-06 5:16 AM
But it doesn't make sense to me.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.