STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Generate code button not doing anything

Hi! allI may not be at the right place but since I can't even start on the CubeMx, here it is.I'm a long time user of Microchip PIC product but since this is my first attempt to use the STM32 I suspect I will have some big time to understand all it's...

Dany0 by Associate II
  • 8185 Views
  • 9 replies
  • 0 kudos

Resolved! STMCubeMX Code Generation Fails on Linux

Hi, I'm experiencing some issues on Linux with code generation in MX. The system I'm running is:STM32CubeMX version 6.12.1Pop!_OS (Ubuntu based) version 22.04Generating code for a Nucleo-H755ZI-Q [although I doubt this matters] Specifically, when cli...

Resolved! Default system clock on NUCLEO-F767ZI

Good morning, in the user manual "STM32 Nucleo-144 boards" is written that the HSE clock is linked to a 8 MHz oscillator. But when I enable the HSE clock in the .ioc file, the value is 25 MHz. I don't understand if the HSE clock is 8 MHz or 25 MHz. T...

GGran.2 by Associate III
  • 7654 Views
  • 14 replies
  • 3 kudos

Resolved! Custom Linker Script with CubeMX

Hi there,I would like to customize the linker script generated by CubeMX.Right now, any changes to the linker file get overwritten when I generate code from CubeMX.Is there a way I can accomplish this? Thanks!

PMart.1 by Associate III
  • 8524 Views
  • 5 replies
  • 1 kudos

Resolved! CubeMX support for HSI clock source for USB

CubeMX is mostly intended for (or mostly used by) noobs. Noobs are most likely to want to skip an HSE for any reason whatsoever, as it adds complexity to a learning process. So it would be nice if CubeMX would accept HSI as a solution for USB clock s...

mo_FEAR by Associate
  • 2241 Views
  • 3 replies
  • 3 kudos

HAL PCD for USB Data Transfer

Hi,I am using an STM32F746-Discovery Kit with a Prophese GenX320 event-based camera.I am using the demo applicaiton provided by Prophese as a skeleton for my code. The application takes captured events from the camera and displays them on the STM's s...

Resolved! X-CUBE-EEPRMA1 package activation in CubeMX

I am in work with a product firmware with STM32G030k8 with additional EEPROM M24C04 I coudlnt ble to instal the driver files . Is this the righ tway am doing,can any one please address this?I am not able to hightlight or install Thanks.

meena_0-1726984378397.png
meena by Associate III
  • 7415 Views
  • 17 replies
  • 2 kudos

Resolved! Configuring a peripheral without all pins assigned

Hi Guys,is it possible to configure a peripheral in CubeMX without assigning all the pins (usually) required for that peripheral. This is a quite typical scenario, if a peripheral is used other than originally intended.E.g. I like to use I2S for effi...

dfrejek by Associate III
  • 3250 Views
  • 6 replies
  • 1 kudos

Problems using CubeMx in uVision

Hi.I am trying to create STM32G0 projects with the uVision IDE, but the configuration option using CubeMX does not work. When creating a new project in uVision, and selecting the STM32CubeMX option within Manage Run-Time Environment, CubeMX does not ...

Kolkentu by Associate II
  • 3647 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.