STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Error FR_NOT_READY with SDMMC on STEVAL-STWINKT1B board

Hi everyone,I'm trying to manage the writing and reading of files on the SD card of the STEVAL-STWINKT1B board, but when I run an f_open it gives me FR_NOT_READY, I've tried with different SD cards but the result doesn't change, I ask if anyone has a...

Luca4_0-1730546238620.png Luca4_1-1730546257603.png Luca4_2-1730546280063.png Luca4_3-1730546297071.png
Luca4 by Associate II
  • 1677 Views
  • 3 replies
  • 1 kudos

Resolved! SPI2 Frequency of the STM32F469BIT7

EMB1428QSQ/NOPB is used which has the frequency of the 1.1MHz fclk and the SPI2 of STM32F469BIT7 is going as a clock to it. I need the minimum value of the SPI2 master that can be fed to the EMB1428QSQ/NOPB. Also, where can I find the minimum frequen...

Cannot install middleware

Hi  I am using STM32 CubeMX and am trying to add the LoRaWAN package but have this message ( see below). I am not sure how to fix ?Any one have any guidence on this? 

Screenshot 2024-10-31 at 21.43.07.png
fabltd by Associate III
  • 1104 Views
  • 1 replies
  • 0 kudos

MQTT over MbedTLS for AWS

Hi!My goal is connection of STM32 mcu to Amazone web service.I was wonderful bu Cube and generate a first application (freertos with lwip) for nucleo-f767zi board. There are function like mqtt_client_connect and mqtt_publish in code that was generate...

SZhuk.1 by Associate II
  • 5912 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.