STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! CubeMX LWIP ethernet_link_thread bug

I am using stm32f407zg board with DP83848 ethernet PHY chip. CubeMX generates code with LWIP for FreeRTOS. App used to answer ping successfully when it starts with connected eth cable only and stops after its reconnecting. After some investigation i ...

el_d by Associate II
  • 12790 Views
  • 12 replies
  • 4 kudos

Problems creating a relocatable git project

I am desperately trying to seed a production project involving multiple engineers (and across multiple companies) and am having great difficulty getting the project to build once it has been pushed to a git repository.  The difficulty involves the cr...

zcab911 by Associate
  • 988 Views
  • 1 replies
  • 0 kudos

Resolved! Newbie with newbie problems Oscillator start up ?

Hi People, for the since start of year i've been setting up boards with Texas C2000 , and for the past 6 months infineon tri-core processors.  I may be changing jobs and it involves STM32 so i'm getting a head start. I have a STM32373C-EVAL , as i ne...

John_S_0-1726412883613.png
John_S by Associate II
  • 8670 Views
  • 16 replies
  • 4 kudos

Resolved! DSIHOST disabled in CubeMX for STM32F469...?

[SOLVED - I found the solution after posting]Hi,the STM32F469 has DSI but when I try to enable it in CubeMX it shows in Italic and greyed out and if I click on it cannot be enabled. See screenshots below.Why is that?How do I enable it?Thank you  

Ricko_1-1729917685233.png Ricko_0-1729917542498.png
Ricko by Senior III
  • 1203 Views
  • 1 replies
  • 0 kudos

CubeMX fails to generate project on apple Silicon

Hello, The project generation for CubeIDE fails on apple Silicon due to x86 compiled libraries org.eclipse.equinox.launcher.cocoa.macosx.x86_64_1.2.800.v20231003-1442/eclipse_11802.so' (code signature in 66ADAB06-1B30-301C-8ECA-7EDC8C31724D '/Applica...

Cordic Two Config

Hi,How can I set up two Cordic Configuration, because I want to calulate using two different function. CORDIC_ConfigTypeDef sConfigSine;CORDIC_ConfigTypeDef sConfigPhase;CORDIC_ConfigTypeDef sConfigCosine; I tried to set up 3 different cordic configu...

James613 by Associate II
  • 964 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.