STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! CubeMX bug when configurating ADC for stm32u031

Hello,I get error messages in Cube MX trying to configure the ADC in STM32U031F6Px to Not Fully Configurable.To reproduce:Start a new project, choose STM32U031F6P6 as MCUGo to ADC, check any channel (e.g. temperature)Change sequencer to "sequencer se...

Resolved! DevEbox in CUBE IDE

Hello! I'm new to the Cube IDE and i want to work with the Chinese board DevEbox with STM32H743VIT6 on it. Before i worked with Arduino Framework where i tested the sd card, ethernet and other basic functions. I wonder, if it and how it possible to u...

STM32CubeIDE hangs while attempting to open .ioc file

I have intermittent problems in STM32CubeIDE 1.8.0 opening a .ioc file. When I double click on the file in the Project Explorer, I get a progress bar titled "Loading IOC". When things are working well, as soon as that bar fills up, it is replaced w...

msch by Associate III
  • 12612 Views
  • 12 replies
  • 4 kudos

new IDE&MX setting baud rate wrong at stm32h743vit

Hi,I have updated IDE and MX, and found that the usart buad rate setting is wrong: setting 115200, but actually baud rate is 57600 (half setting). Is it new ST firmware error or not? I am not sure that the other clock settings is right. Please help t...

bjrobert by Associate
  • 1505 Views
  • 2 replies
  • 0 kudos

Resolved! CubeIDE 1.16.0 (MX6.12.0) STM32G0B1CCU ADC1 poblem

Hi,I have tried to load a Project (.ioc file) build with CubeIDE 1.15.0 in the newly released CubeIDE1.16.0 (with CubeMX 6.12.0).This give me an error on ADC1:1) I can't select Vbat as ADC source (as working on CubeMX 6.11.0)2) I get a warning about ...

ADC1_problem.jpg
MHoll.2 by Senior III
  • 2817 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.